Part Number: LMH34400
Hello team,
My customer would like to sense photo diode (transimpedance circuit) with single supply OPAMP.
However, if the Opamp is operated with single supply, it will require bias voltage because if the photo current = 0A, then the output will be out of comon mode range.
I have found LMH34400, and it is single supply, no Bias voltage needed for transimpedance operation.
Is this device usable without any bias for Photodiode? On the datasheet, the Kathode of photo diode was connected to -Bias voltage.
Can LMH34400 operate with wy customer's photo current spec below?
- 50nA max
- 10pA at dark current
- Few kHz frequency pulse current
Best Regards,
Kei Kuwahara