Part Number: INA159
Hi team,
I didn't find the recommended PCB layout for INA159 in user manual or other documents.The 5 and 6 pins of the its output are directly connected in the circuit.
Do I have these two pins copper poured in the PCB, or connect them by wires (there will be sharp angles during the backend), connect the 5 pins to the 6 pins at right angles?Which one is better?
Also, If I put an RC low-pass filter on the output to connect the ADC (one of the typical applications in the manual),What should be the placement of the RC? Is it a good idea to have capacitor for RC close to the ADC pins rather than to the INA159?