Part Number: LT1013D
Other Parts Discussed in Thread: TLV2387, OPA2196
Hi Team,
I have an existing disign using LT1013DIDR, current power supply of LT1013DIDR is +5V to GND, the issue is when input is 0V, output is not 0V.
I plan to change VCC- pin to negitive voltage, but there is no -5V on the board, only -12V, also don't have +12V.
Queston is can I use +5V for VCC+, and -12V for VCC-?
Thanks in advance.