Part Number: TLV3801
I am using the TLV3801 as a signal conditioner into the PCB however the input signal has changed.
Previously I was using to convert LVPECL signals to LVDS however now I need to convert CMOS (0 to 3.3V) to LVDS. This, based on the datasheet, means I now need a Vee = -1.5V since i am converting 0 to 3.3 to 0 to 1.5V and using a DAC output to provide a reference of 0 to 1.5V to the negative input.
However, my problem comes that my current board is designed with the Vee and Thermal Pad to be connected to ground. I would like to prototype this on this current board, as a re-spin will add significant cost and I would like to de-risk this complete circuit operation. My question is what a better option is since the thermal pad I can't easily connect it to Vee as it has vias in pad:
1. Connect Vee to negative -1.5V and leave thermal pad connected to ground - I know this can cause some leakage?
2. Connect Vee to negative -1.5V and back drill the vias into the thermal pad to remove ground connection?
I understand neither solution is optimal but i would like something that work for now and in the next re-spin will go for performance.