Other Parts Discussed in Thread: XTR300, XTR111
I am new to using these types of devices and am trying to get a simple test set up to explore the features of them. When following the documentation for the device it calls for a two supply for each of the examples, however I do not have one available to me. Is there anyway to set this device up to use a standard 24V variable power supply to get a basic test going to explore the functionality of the device and get a better understanding of how it works. If there is not is there another device available that would be a fit in this application.