Other Parts Discussed in Thread: OPA828
Hi TI team
Few questions need help on OPA928:
1. When this part will be officially released?
2. What is the supply volage range? Is it max only 16V? Some overview shows it can operate upto 36V? I’m bit confused about the allowed 40V VDDmax but 16V recommended, maybe the Ib looks worse then.
3. If this amplifier cannot operate at high voltage is there any alternate amplifier from TI that can be considered offers extremely low input bias current (< 20 fA). My requirement is an op amp upto40V and with leakage lower than 100fA across entire temperature range.
Appreciate some feedback and suggestions here.
Regards,
Bharat