Part Number: VFC110
Hello
We have some Signal Isolator using VFC110 with Fiber Optic Interface for shipment to France.
I can share the full Ckt if you want, but basically a TIA followed by V to F , transmission thru' FO
and on receiving end a F to V , followed by Butterworth Filters and level shifting for 0-10 to 0-10 V
Multiple cards are inserted in a 19 Inch Rack and the whole system works on 230 V AC .
Several such 19 Inch Racks with Cards have been tested for EMI/EMC , IEC 61000 Series for CE, RE
and immunity to Surge .
All have passed those tests successfully
Our clients is apprehensive whether the surge tests may have weakened the IC's such as VFC110
and wants a positive confirmation from the Horse's mouth, so to speak.
The 0-10 V Input is first passed thru' a TIA before being applied to the VFC110, so any surge is first taken by the TIA.
and the Power Supplies have adequate protection in the design to enable them to pass those tests.
Would someone be able to confirm that the IC's have not been degraded or any reduction in their expected life
The IC's are fully functional as such including the Internal Cos and Res.
Thanks and regards
Varun