Other Parts Discussed in Thread: INA240, INA300
Hi Everyone,
I wanted to know if I can use the INA181 for inline current sense.
Usually I will use it in the low side but I am driving a DC motor with an IC with integrated FETs so it is not possible.
My supply is 11V so it should be OK as the Common mode range is up to 26V.
If I'll set the Ref voltage to be 0.5 VCC it should be OK if I understand correctly right?
Alternatively, if this part cannot be used for inline current sense, can you offer a device that can and is cost effective.
I don't need high accuracy and the system is cost sensitive so device like INA240 are too expansive.
Thanks,
Tomer