Other Parts Discussed in Thread: THP210
Hi ! I want to add differential offset to ina 851 in two different ways.
The first is an offset that is added differentially directly to the output, not multiplied by the gain.
The second is an offset multiplied by the gain and added differentially to the output.
I cannot add it with Vocm or Vref pins because the receiver system also has a differential input and the offset common mode signal I add to the Vocm or Vref pins will be accepted and deleted.
any idea?