Other Parts Discussed in Thread: AMC3302, TPSI3050
Related to E2E thread here, I would like to understand what is the switching frequency of the DC/DC converter inside the AMC3330 and AMC3302.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brandon,
It should be 30MHz. Please see this tech note for more information on this topic as well.
Best regards,
Eva
The inquiry is due to emissions issues.
The customer has an issue with EMC compliance for CISPR25 which uses both the AMC3330 and AMC3302.
The emission results show exceeding all limits for the CISPR25 FM range near 89MHz center frequency. The design also has a TPSI3050 (see other E2E thread) which may be the contributor for the 89MHz.
However, for the AMC3330 and AMC3302, they see peaks at 31MHz and ~93MHz.

The tech note you provided mostly references CISPR11. Do the same techniques apply for mitigating for CISPR25? Or should other methods be used?
Hi Brandon,
Yes, they could try the tech note recommendations. The mitigation techniques should get similar results for CISPR25. If it wasn't referenced to be tested for CISPR25 though, we just cannot guarantee the same results.
Best regards,
Eva