Part Number: THP210
Hi,
I planning to use THP210 IC for single-ended signals to differantial signals. Single-ended signals are max. 5V. I need to max. -+8V differential signals. So, I have to adjust the gain of THP210 according to 3.2 V/V. I simulated THP210 IC at LTSPICE. I see, This is possible according to LTspice simulations.
I need to try this IC, but I don't have THP210 IC now. I just want to know the accuracy of this output. Is it possible to set the gain of THP210 to 3.2 V/V?