Other Parts Discussed in Thread: THS3092, BUF634, OPA564
Dear Experts,
I need your help to find a suitable IC. I need to actuate a piezo at its resonance frequency of 2.4MHz. Please suggest an IC to operate in either series or parallel resonance for maximum wave transfer. I have no clue on which mode it should be operated to get maximum wave transfer or vibration. I need flexibility to change the input signal. (up to 3MHz)
Other Info:-
1. Target Input supply voltages and current is 24V 5A.
2. Target input signal frequency 3MHz(max) and Vin magnitude 5V (max).
3. Target output signal frequency 3MHz. (Voltage and current according to operation mode Series or parallel Resonance)
4. Piezo will be connected through a cable externally.
Regards,
Yash.