Other Parts Discussed in Thread: LM2903B, LM2903, LM339, TLV1812
Hi Staff
I have a question regarding the contents of the LM2903B-Q1 data sheet (SLCS141L).
A time summary of TR and TF is shown on page21 Response Time.
• The rise time (τR) is approximately τR ⇒ RPULLUP × CL
• The fall time (τF) is approximately τF ⇒ RCE × CL
– RCE can be determine by taking the slope of Section 6.14 in its linear region at the desired temperature,
or by dividing the VOL by Iout
Question 1.(LM2903B-Q1)
Figure 3-38 L to H rse time takes approximately 1us.
I think it is necessary to set Rpullup and CL to small values in order to make this rise time steep.
What do you think?
Figure 3-38 I want to set the L to H time to the same rise time as Figure 3-37 H to L.
Question 2.(LM2903B SLCS005AF)
I think this device is an open collector output comparator, and the output rise and fall times are determined by the sink current, Rpullup, and CL.
Figure 6-4 and Figure 6-5 transition at the same time.
Please tell me the power supply voltage, Rpullup, and CL to achieve this waveform.
The waveform in the figure looks like a push-pull waveform.
best regards
cafain