Part Number: OPA211
I cannot see which end of the OPA211 SO-8 chip is pin 1 and 8, and which end is pin 4 and 5? See attached photo.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA211
I cannot see which end of the OPA211 SO-8 chip is pin 1 and 8, and which end is pin 4 and 5? See attached photo.

Hey Henrik,
I agree with Clemens answer. Let us know if we can be of further assistance.
Best Regards,
Chris Featherstone
OK. There seems to be an almost invisible printed dot and a slightly bevel edge, which both correspond to each other and to the direction of the almost invisible letters... But in that case the only really visible symbol is next to pin 8. So you are not making it easy. ;-)
Now I have added the pin-1-dot that would have been nice to have. ;-)
It's incredible what the camera in an old cheap smartphone can do under good light conditions.