Part Number: OPA567
Hi,
There is damage issue with high temperature.
With start, it works well but output gradually get worse and there is no output finally.
For LD operation, V+: GND, V-: -3.3V
The questions are:
1. if V- supply current rating is lower than requirement, it means V- supply voltage is not regulated. in this case, can OPA567 get damage?
2. if yes, could you explain why it get damage?
3. Now EP(pin13) is connected to GND. Is it ok that V+ also connected to GND?
Schematic is as below.

Thanks.