Other Parts Discussed in Thread: OPA855, OPA858
Dear Specialists and TI users,
In past when implementing Photodiode amplification stage for VLC I usually used a transimpedance amplifier such LMH6629 and then use a high speed comparator set at Vref.
However here I need to amplify very small current at the order of nA or tens of nA from S1223 Photodiode (Cp = 10pF) and remove DC bias. For such small current the voltage variation at the output of the TIA is too small in order to connect directly the comparator.
I tought to use Voltage amplifier in cascade but I am afraid of the noise figure and also would tought how removing DC bias regarding ultra small AC variation (f=2MHz).
If possible for you of course, I would really appreciate to have your advice on these question.
I wish you a nice day,
Yours,
Simon