This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3217: DAC3162

Part Number: THS3217
Other Parts Discussed in Thread: DAC3162,

Hello, engineers:
I would like to ask a question. I am designing a circuit using DAC3162 and THS3217. I notice that the datasheet for the THS3217 labeled the input common-mode voltage range for the D2S stage of the device as -1V to 3V. where the datasheet states:“The 3-V maximum common-mode range is intended to support DAC supplies up to 3.3 V, where the average output operating current pulls down from 3.3 V by the termination impedance from the supply. For instance, a 20-mA tail current DAC must level shift from a 3.3-V bias on the output resistors down to 3 V or lower. This DAC-to-THS3217 configuration requires at least a 300-mV dc level shift with half the tail current in each side, implying a 30-Ω load impedance to the supply on each side of the 20-mA reference current.”

Coincidentally the DAC3162 is supplied at 3.3V and configured with a tail current of 20mA in my design, which means I'm going to define the impedance matching of the THS3217's input stage to be 60 ohms or more to control the input common-mode voltage within the range. I note that this input common-mode voltage range (-1V to 3V) is confirmed with the D2S stage of the THS3217 device supplied at ±6V. Considering that the input common-mode voltage is related to the supply voltage, if I increase this supply to ±7.5V, will its input common-mode voltage range be able to continue to expand? Further, can this common mode voltage be capped above +3.05V for normal use with 50 ohm impedance matching?

  • Hi Zenan,

    The device's input common mode range will increase with increasing supplies like you mentioned. However, if you are trying to get +3.05V at the outputs of the DAC you should have no problem from the THS3217's perspective as its common mode range extends well beyond 3.05V at a ±6V supply so there should not be a problem setting this common-mode and sticking with ±6V supplies. I would confirm the DAC's output compliance range is not violated which it appears it's not at 3.05V.

    Best Regards,

    Ignacio

  • Hi Ignacio,

    Thank you very much for the quick reply to my question. I appreciate it. The compliance voltage range of the DAC3162 is [AVDD-0.5V,AVDD+0.5V], here AVDD=3.3V. The DAC3162 is a current sinking DAC constructed from a NMOS array. So when the tail current is set to 20mA, the voltages at outputs IOUTP and IOUTN in the digital code of "0" are 3.3V-10mA*25ohm=3.05V, which is same to the common-mode voltage. This is how I deduced it, I don't know if it is correct?

    In my design, to be on the safe side, I set the D2S stage supply voltage of the THS3217 to ±7.5V (The upper limit is ±7.9V), which is higher than the ±6V in the datasheet.Thanks again for your answer!

    Best Regards,

    Zenan Shi