Part Number: AMC1350-Q1
Other Parts Discussed in Thread: AMC1350, AMC3330
Hi,
I have recently created a design using the AMC1350QDWVRQ1.
On the component datasheet and therefore on numerous comparison/supplier websites the component is listed as having SOIC-8 packaging. However, the actual packaging is SOIC-8 Widebody. This information can only be found in the footprint drawing at the bottom of the datasheet, only when looking at dimensions.
This is the same with a large amount of datasheets in the AMC series.
I would suggest a change to the datasheet(s) where the term "wide" is added to the package.
In addition, I am wondering if anyone could offer a TI or third-party differential voltage sensing (±2.5V peak-to-peak input voltage) isolation amplifier that has an SOIC-8 (narrow) package and the same pin layout as the AMC1350.
Any help would be appreciated.
Thanks