Part Number: AMC22C12-Q1
Other Parts Discussed in Thread: TPSI3050
My application will use the AMC22C12-Q1.
I plan to activate the Latch function of the AMC22C12-Q1 with a delay to the enable signal of the MOSFET activation that is done with TPSI3050.
This delay of the Latch function is planned to be done with an RC that has a time constant of max 1ms.
Is the latch input of the AMC22C12-Q1 able to cope with this "slow" rising/falling input signal of approx 3V/ms?
Note: The datasheet does not require here a min. voltage slew rate.