Other Parts Discussed in Thread: INA148, INA592, INA149
Hello,
I plan to use this as part of a current sense amplifier circuit due to its wide Abs max for inputs and high common mode range.
For 48V reverse polarity, the part is unpowered (and its input is RPP protected through an ideal diode ckt)
However the inputs can backfeed thru input resistors across current sense resistro (shown on right 200uOhmx2).
However abs max shows +/-200V on input regardless of input voltage.
So if there is no power supply under RPP condition, the inputs will survive this condition, correct?