Other Parts Discussed in Thread: XTR115
Hi,
I think I can use teh XTR115, it seems one of the best transmitters.
But I need to improve the temperature stability; drift.
As far I have calculated the device is for a 100 degrees temperature drift
typical 0.0475% and maximal 0.275%.
The datasheets give no curves about the offset and gain drift, so I don't know
how to compensate it.
Is there additional data available about the temperature drift behavoir?
Is it a repetive curve or rather random?
Typical the device will suite my requirements, But wat is the spreading between
several devices?