Part Number: INA901-SP
I have an application that will input more than 5mA into the IN+ and IN- pins of the INA901-SP. Do I need to add external resistors to decrease the input current below the absolute max stated in the datasheet? Due to offset errors with two individual resistors I assume I would need to get two resistors on the same die. What is the best way to solve this issue?