Other Parts Discussed in Thread: TLV3601, TDC7201
We are using TLV3601/03 EVM for ToF measurement.
Detector output signal connected to Non inverting terminal and a ref voltage at inverting terminal of TLV3601.The out of TLV3601 is connected to TDC circuit as Stop pulse.
Issue - TLV3601 output signal (around 2V ) is highly attenuated (around 100 mV) while connecting to STOP pin of TDC and TDC is not consider it at transition pulse for time measurement.
Further few more clarifying questions:
- TLV3601/3 EVM board have few zero ohm resistors as per EVM Schematic. Which are to be populated in case of TLV3601DCK comparator IC.
- Any care to be taken with regard to reference voltage for TLV3601
Thanks