Other Parts Discussed in Thread: INA2143, , AMC1350, AMC3330
Dear Sir and Madam,
I am currently designing an isolated amplifier circuit, that is capable of measuring a high voltage signals up to 1500 V with at least of 20 kHz bandwidth. The high voltage is divided by factor of 1001:1 (voltage divider with 1Meg and 1 kOhm) and resulting signal get feed to the input of the AMC1311B. The differential output signal of AMC1311B get feed to one half of INA2143 amplifier, to get 10x amplified single side output signal, which I have finally connected to scope input, using the shielded BNC cable. After the prototype board was build, I have measured the noise performance of the whole circuit. I have found in the output signal the high frequency broadband noise, starting from about 50 kHz, with a broad peak at about 300 kHz and a high sharp peak at about 623 kHz, please see the attached picture. The signal output is bandwidth limited to 150 kHz due to INA2143 bandwidth.

The blue signal is the output from INA2143, the red signal is the +5 Volt VDD2 supply of AMC1311, measured at 100 nF blocking ceramic capacitor, both signals were AC-coupled. The VDD1 was supplied from 3 alkaline batteries (4,6V), because I was thinking the VDD1 supply was producing additional noise (I have disconnected the VDD1 DC/DC converter and unpowered it completely). It's a pity, that the AMC1311 datasheet does not show the whole noise picture up to 1 MHz in the Fig. 7-23. To support the circuit designer, the datasheet should be improved, in order to show the whole noise picture.
To get reed of the high frequency noise above 100 kHz I will use a low pass RC-filter, with a filtering frequency, starting from 20 kHz.
After I have changed the scope resolution, I have found some strange spikes in the INA2143 output signal. The next FFT spectrum shows two peaks at 2,64 kHz and 3,41 kHz, which are present at lower frequencies and limiting the AMC1311B noise performance. The peaks also can be seen in previous FFT spectrum.

The input signals are the same, as described in FFT-spectra above.
Are the peaks at 2,64 kHz and 3,41 kHz typical for the AMC1311B output signal?
In the Fig. 7-23 of datasheet, the both peaks can be hardly recognized, because of the logarithmic scaling of frequency axis and not enough averaging/signal accumulation time.
Are the same noise features also available in ISO224B, AMC1350 and AMC3330 isolation amplifiers?
If the peaks are typical, how one can reduce them?
Thank you in advance,
Dr. Evgeniy Zubkov