This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6521: How to connect channel B if only channel A is used?

Part Number: LMH6521


Hello guys,

I have an application with this specific IC (not changeable), but only one channel (A) out of the two should be used. I searched in the datasheet, on how to connect the unused channel B at the inputs, outputs and B0...B5, LATB, so it does not swing or affect the other channel A. 

I found out, that the inputs are internally biased to 2.5 V and the outputs are biased to ground. So does tht mean, I can left them floating? Or is it recommended to strap them to a certain voltage level with a resistor of some xxx kOhms? For the B0...B5, I assume, GND connection is fine, as well as for the LATB Pin?

Anything else to consider?

Thanks in advance.

Philipp