Other Parts Discussed in Thread: LM339
Hi,
Chen tieing the 2 output ports together, I get only 1.5V on the output if only one of the inputs are high. When high on both inputs the output is 5V. Previously I was told I could just tie the 2 output ports together to achieve an OR function. Could you please advice on what I have done wrong in this case (see attached screnshot from design). I guess I am missing some diodes, but would like your opinion.
Best regards, Kenneth