I am attempting to create a photodidoe amplifier circuit used for detecting fluorescence from an atomic source and cannot determine the type of buffer/follower OP AMP I should use when trying to convert the high impedance from the photodiode circuit to the low impedance necessary for the 50 Ohm BNC cable. I am currently considering BUF602 or BUF 634, but am open to other suggestions. I have attached a drawing of the circuit.