Other Parts Discussed in Thread: TLV9001, LM321LV, LMV321A, TLV8801, OPA333,
Hello,
I need a voltage to current circuit to power a tiny LED from a DAC. DAC output is 0 - 2500mV. The LED has a Vf of 2.85V. Supply voltage (V+ in SLAU502) is 3.3V but I can also make it 5.0V if needed.
I implemented the circuit in SLAU502 and I think I can leave everything the same except the last stage. Since I only want 1.0mA maximum, Equation 9 is:
RS3 = (Vrs3) / (Iload)
RS3 = 470mA / 1mA
RS3 = 470 Ohms
Is this correct? Or should I have changed the first stage too?
Thanks,
Derek