Other Parts Discussed in Thread: CC3235SF,
We are currently using the TAS6422Q1 and TAS6424Q1 amp devices. We are running into problems on
24vdc systems that shut the parts down when PVDD hits around 27VDC. This voltage could easily be
seen in most dual series 12vdc battery applications when the alternator kicks in to charge.
So my client asked if there were any newer parts that could withstand at least 30vdc as PVDD out there?
Found this:
TAS6584-Q1
Which looks great. Would love to compare the data booklet to the part we have now to determine how
much work it will be to blast out a new design with the newer part. We also will switch from the CC2642R1
MCU to the CC3235SF MCU for control and drive the AMP with I2S. Our board uses 3 AMP chips for
driving the loads.
Initially I need a like to gather up the full data book to evaluate them will get the eval. board, etc..
Also any info. on what stage this part is in. I see Mouser has over 2K of them so must be production?
Thanks, Marc