Part Number: TLV6001-Q1
Other Parts Discussed in Thread: TLV9001, , TLV9001-Q1, INA180-Q1
Hi,
The customer experienced a problem with the operation after configuring the circuit.
The circuit increased R101 (Rshunt) from 0.1 ohm to 1.4 ohm, but it does not work.
Is it the same problem as offset error?
It seems to work only when it is increased to approximately 5 ohms or more.
Are there any circuit problems?


The circuit shows the difference when changing as shown below.
R106 = R107
R108 = R109

The behavior depends on the R106 (=R107) Value.
Please advise what kind of difference there is depending on the value of R106(=R107).
And, customer changed it to TLV9001 and tested it, but it was not resolved.