This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4170-Q1: circuit

Part Number: OPA4170-Q1


Hi..

I want to design a op-amp circuit, with single output pin.

Input :- 0V to 5V

Output:- -10V to +10V

 at 0V input output will be -10V and 5V input output will be +10V