Other Parts Discussed in Thread: OPA361, , OPA316, OPA858DSGEVM, THS7372, THS7368, THS7364, THS7360
Dear Team,
we have some design questions regarding OPA360/OPA361
1) If the OPA needs to be enable all the time is it better to leave enable pin floating or tie directly to V+ ( 3.3V)?
2)If the SAG function of OPA360 is not used, what is the proper termination of this pin
3)if the Rset function of OPA316 is not used, what is the proper termination of the pin, floating or tie to GND?
4)Please can you recommend decoupling caps for the V+ pin @ 3.3V ? do we need to filter this supply with inductor or ferrite bead?
5) Her is or reference schematic but it is for AHD, and we only need to use CVBS and thus want to replace TPF140 with OPA360 / OPA361
6) we want to use following ESD diode to replace GBLC03CI, is it ok?