Part Number: INA199
Other Parts Discussed in Thread: INA190, INA191, INA186
Hi team,
ASUS now want to use the INA199A3DCKR material and connect the Supply Voltage, IN+, and IN– pins to DC_IN 24V. Calculated based on a tolerance of ±5%, the voltage will reach 25.2V. However, the maximum voltage of
the Supply Voltage, VIN+, and VIN– pins in the datasheet is +26V, is there any risk in using it like this?

BR,
Comi