Part Number: PGA309
Hi,
I use PGA309 to detect Strain Gage Bridge changes.
In many projects conducted with PGA309, the Strain Gage Bridge supply voltage appears to be 5V.
For this reason, Vin1 and Vin2 inputs will be 2.5V in a zero-strain state.
The supply voltage of the Strain Gage Bridge I will use appears to be 10V. We must use 10V voltage for the Strain Gage Bridge. This cannot be changed.
For this reason, Vin1 and Vin2 inputs will be 5V in a zero strain state.
When the VSA supply voltage of the IC is 5V, Linear Input Voltage Range VSA − 1.5V = max 3.5V as stated in the datasheet.
For this reason, the situation where the Strain Gage Bridge is supplied with 10V is not suitable for PGA309.

To ensure this compatibility, we plan to reduce the 5V value at the Vin1 and Vin2 inputs to 2.5V levels with Opam+Voltage Divider and read the Strain Gage Bridge with 10V supply using 2 Gain in the PGA309.
When only a voltage divider is required, it disrupts the Strain Gage Bridge structure. For this reason, Buffer Opamp was used. I sharing the circuit below.

If you have a different and effective solution to this issue, I would be very happy