This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV316-Q1: Linear Full Scale Range input for TLV316-Q1

Part Number: TLV316-Q1


Hi all,

What should be the linear full scale range input for TLV316-Q1 ?

I'm planning to use this Op-amp for high voltage measurement and so, I'm confused on understanding the minimum input voltage that should be provided at the non-inverting terminal of TLV316-Q1 so that the device operates in linear region. And what is its gain. Is it fixed at unity most of the times ? It would be helpful If someone could point out a reference design for high voltage measurement using TLV316-Q1.

Please consider this query ASAP.

Thank You

Naveen Johny