Part Number: AMC1350
Other Parts Discussed in Thread: AMC1351, AMC3330
Hello TI Team,
I am currently in the process of designing an AC/DC voltage sensor utilizing the AMC1350 isolation amplifier and would greatly appreciate your expertise in verifying the schematic and associated values.
1)One aspect that has given rise to uncertainty pertains to the output low pass filter. Specifically, I am seeking guidance on how to appropriately select a low pass filter that accommodates a switching frequency range of 15-25kHz, while also addressing the 50/60Hz fundamental frequency of the system.
2)The schematic provided illustrates that the sensor is designed to measure phase to neutral voltage. However, should the need arise to sense phase to phase voltage, I am keen to understand how the schematic might require modification to accommodate this requirement. If I add separate isolated power supply for each phase sensor could that help.
3)Can I use AMC1350 isolation amplifier for Battery voltage sensing or should I use AMC1351, which any way it is unidirectional. But I'm having concern if I want sense reverse voltage. How could I sense it?
Given the criticality of this application within the industrial UPS sector, ensuring the accuracy and reliability of the voltage sensor design is paramount.