Hi team,
Could you help with this? Customer setting OCP around 12A.
But when the current up to 4.4A will trigger the OCP point. could you give some suggestions? thanks


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you help with this? Customer setting OCP around 12A.
But when the current up to 4.4A will trigger the OCP point. could you give some suggestions? thanks


Hi Jimmy,
I doesn't look like the out pin is fully transitioning. The expected behavior would be for the out pin go low and stay there while the input voltage is above the reference voltage.
A few questions:
1. What is happening with the OC_LATCH signal?
2. Are the VDD1 and VDD2 voltages of the device stable during the above transition?
3. Could you provide a zoomed in scope capture of the out pin behavior seen?