Part Number: ISO224
Hi Team,
My customer has the below queries on ISO224B. Please help in clarifying the same.
1) As per data sheet absolute maximum voltage for primary side power is 26V. What happens when we exceed this voltage? What kind of failure happens inside IC? Will failure in primary side effect circuits in secondary side of isolation amplifier?
2) We have inadvertently given a voltage of 65V to primary side power and IC had failed. We have decided to replace the IC as well as the input side bypass capacitors. Is there any chance for this voltage to propagate to secondary side? We are using 50V rated capacitors. Should we change the secondary side bypass capacitors also?
Thanks,
Jash