This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2992: Asymmetric power supply for an opamp

Part Number: OPA2992


I'd like to power the opamp with +22V/-5V power supply. The OPAx992 (and similar) specify the power supply to ±20V or to 40V. In my case the input and output are in the range from -1V to about 18V (I need to use it as a follower and maybe also as a 2-4 gain amplifier for positive signals). The datasheet only specifies that (V+) – (V–) should be less than 40V (which is true in this case) but doesn't mention other details about asymmetric power. Are there some other downsides of using it like this.

Thanks!