Other Parts Discussed in Thread: INA190
I'm designing a precise high side current measurement circuitry which needs to switch measurement shunts through a few measurement ranges (that part is mostly done). I noticed that INA241A, while having all other parameters seemingly perfect for my use case (bandwidth, error, gain options, common-mode voltage...) has input bias current of 25-45uA. Does that mean I wouldn't be able to use it to measure shunt current in uA range. My common mode voltage is between 0 and 18V and power supply is 5V (although I have other higher voltage rails, such as 20V, as an option for powering it). If that's the case is there a way to improve it (maybe add some high input impedance buffers to Vin+ and Vin-) or would I need to use a different amplifier?