Part Number: OPA2192
Other Parts Discussed in Thread: OPA192
Dear Bu friend,
My customer used OPA2192 reference output deviation.The input is 2.5V and the outputs are 2.5V and -2.5V respectively.
Here is the follower circuit.

Here is the reverse amplifier circuit

Test method: Use a six-and-a-half-digit multimeter to collect the reference voltage and op amp output voltage, and power on multiple times to record the values (the following data selects data with large numerical deviations)
| Input(V) | Follower: +2.5V | Reverse:-2.5V |
| 2.49987 | 2.50048 | 2.4931 |
| 2.49987 | 2.49983 | 2.4931 |
| 2.49985 | 2.4998 | 2.49284 |
Could you pls give some suggestion? Does it cause by voffest or the drift?