This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA3221: Measuring alternating current

Part Number: INA3221

Is it possible to use INA3221 to measure alternating current when using TEC controller for peltier cooling? Voltage changes from -15V to +15V(polarity of voltage changes when heating or cooling), current stays under 5A. If not is there a chip that can do that?