Part Number: INA828
Other Parts Discussed in Thread: INA823
➀ Temperature specification compensation of 125°C or more and low temperature drift
② it is possible from a common-mode input range of 0V with a single supply (assuming +5V) vs an output, and from an output of 0V to a minimum of 1.8V.
I am currently using the following devices in the range of +Vs = +5V in the
AD8223, but they are in the same range.
③ SOIC8 pin preferably same as AD8223