Other Parts Discussed in Thread: INA381
Hi Team,
May I know whether I can leverage all three INA381-Q1 and connect them to the same Rsense?
We will connect the VOUT pin to CMPIN pin in each INA381-Q1 and set the different threshold(CMPREF) for each CMPREF pin to get different trigger(/ALERT) condition.
All the /ALERT pins will connect to MCU's GPIO0/1/2.
But since the source is the same so I would like to know whether there is any side effect for such connection.
Like parasitic capacitance or offset current.
Our targeting current through that Rsense is 20mA ~ 100mA.
Kindly let us know if you have any concerns.