This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: PSRR in datasheet vs simulation

Part Number: INA240

I've noticed that the SPICE model for the INA240A1 does not match the datasheet for PSRR. While the datasheet specifies a PSRR of 10 uV/V max, the model is demonstrating 0.5 V/V. As far as I can tell, I've replicated the conditions from the datasheet. Is the datasheet wrong, or is there an issue with the model?