This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA228-Q1: Maximum input frequency

Part Number: INA228-Q1

Hello,

I am interested in using the INA228-Q1 for the power monitoring of a battery pack. The load current is expected to fluctuate rapidly with frequencies up to 40 kHz. Given that the INA228-Q1 has the fastest sampling time as 50 µs, would it be unable to handle this signal? Or having a delta-sigma converter would help in this regards? It would be acceptable for my application If it was averages out the current value within one sampling period.

Many thanks for any suggestions on this.

Best regards,

Roland