Other Parts Discussed in Thread: LM321,
I have a basic op amp circuit diagram consisting of LMV321 and LM321 as shown below. The reference voltage for both OP Amp ICs are 2.5V. The input voltage is 5V. I want to re-design the circuit with 3.3V keeping same reference voltage of 2.5V. So, I basically want to know the design configuration and how the resistor values in the circuit are calculated. I have searched the datasheets of both op-amps, and I am left confused. Could you kindly provide a detailed calculation so that it will be helpful for the 3.3V design. The circuit diagram is shown below.
Regards,
Srinithi