Part Number: OPA4202
Other Parts Discussed in Thread: DAC80004
kindly help me to simulate the below circuit in TINA TI for 0V, 2.5V, 5V, 7.5V, 10V Replace DAC and OPAMP with the Part number mentioned below.
OPAMP-OPA4202ID
DAC-DAC80004

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
This is an identical post to the link below; please see this link for the model requested.
I'll go ahead and close this, if you have any further questions then please ask on the original post.
Regards,
Mike
Hi Michael,
In below loop which you have attached is stimulation for OPAMP only, but we are in need for DAC .
Kindly use the below mentioned part number for DAC and give simulation results.
Hi Nishalini,
What type of analysis are you looking for? Attached is a Tina TI file containing both devices. Note that the DAC80004 can only go up to 5.5V output.
And here is the transient result of this circuit. This shows the DAC going full scale (~5V) from 0V, and how fast the OPA responds to this output change.
Thanks,
Erin