Part Number: INA851
Hello, I am using the INA851 in a 0.4 overall gain, that is Gout = 0.2 and Gin = 2. I am looking for the gain error of this configuration.
The datasheet states:
- gain error is +/- 0.1% with G = 0.2. I am assuming that this is mainly the accuracy of the second stage when set in a G = 0.2 (that is G02+ and G02- connected to their respective OUT).
- gain error is +/-0.02% with G = 1. That looks like the combined accuracy of the two stages in their ideal (best accuracy) configuration
First, I was expecting the 1.25K embedded resistors to precisely match the 5K ones, and when configured in G=0.2 the accuracy would not degrade that much, that is from +/-0.02% to +/-0.2% (one magnitude). Is there something I am missing here ?
Then finally
- gain error is +/-0.2% with G > 10. That would be mainly the accuracy of the first stage with a perfect RG connected and Gout = 1.
For the sake of this discussion, let's assume I have Gout = 0.2 and Gin = 10 (yes I know, there is a better combination), then is the overall accuracy computed by adding 0.1% for Gout and 0.2% for GIn, that is 0.3% total ? (not e that knowing that the overall part performance is 0.02%, I neglect combined effects between Gin and Gout).
If this is not correct, then how should I compute the gain error ?
Best regards
Pascal