We have a pre research project that supports LTE and NR standards. Please help confirm if LMH2110TMX/NOPB can meet the power detection requirements of NR and LTE. Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a power detection chip specifically designed for NR, or is this one that also meets the modulation method of NR for power detection? Currently, the application in this scenario still refers to LMH2110TMX/NOPB, and the power output by PA meets Class2 and Class3. The product is most likely to be used in automotive products

Hello Tony,
Yes LMH2110 can be used for LTE and NR, As it is a RMS detector it can support different modulations techniques. However at higher frequencies like 6GHz and 8GHz it can detect power levels from -20dBm to +5dBm. Can you confirm the frequency bands for LTE and NR?
Regards,
Hruday